Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How can I output a clock signal?

Latest Updated:03/24/2009

Question:

How can I output a clock signal?

Answer:

There are several ways as below.

1. Use PWM

2. Use toggle output of timer

3. Use TMOW pins (its availability depend on each product)

4. Use SCI1 clock continuous output mode 4 (its availability depend on each product).

For detailed, please refer to the hardware manual.

Suitable Products
H8/38602R
H8/38086R
H8/38086
H8/38076R
H8/300L Super Low Power
H8/3887
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104