Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How can I distinguish between Spec A and Spec H M38507F8SP/FP part name?

Latest Updated:12/16/2004

Question:

(MCU Comparison, General MPU/MCU)  How can I distinguish between Spec.A and Spec.H M38507F8SP/FP with the same part name? [2004/12/16]

Answer:

Spec.A and Spec.H are distinguished by marked serial numbers. For Spec. A, "A" is marked on the left of the serial number.
Ex: A0123456

(#104949)

Suitable Products
3850A