Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How can I adjust the light of LCD panels in H8/3802 and H8/38024?

Latest Updated:03/18/2009

Question:

How can I adjust the LCD panels luminance in the H8/3802 and H8/38024 series ?

Answer:

The luminance can be adjusted by inserting a variable resistor between Vcc and V1. Since driving power is supplied externally please set PSW bit to 0
Suitable Products
H8/300L Super Low Power
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3802, 38002S, 38004, 38104
H8/300L
H8 Super Low Power