Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Explain further, RAM content is undefined when microcomputer is reset

Latest Updated:02/14/2006

Question:

The user's manual says "RAM contents is undefined when the microcomputer is reset". Does this apply to a hardware reset during the MCU operation as well? Or is it just for the power-on reset?

Answer:

A software reset never occurs during a RAM write. Therefore, the software reset never corrupts the RAM contents.
On the other hand, the hardware reset can occur when the CPU is writing to the RAM. Therefore, the RAM contents may be corrupted due to a hardware reset. It will corrupt any RAM area, not only at the address where the CPU is writing.
However, because the CPU never writes to the RAM in the stop or wait mode, when the MCU returns from this mode by a hardware reset, the RAM contents are protected even after the hardware reset.
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/38A
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N