Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Does the H8/300H CPU accept nested NMI interrupt requests ?

Latest Updated:03/18/2009

Question:

Does the H8/300H CPU accept nested NMI interrupt requests ?

Answer:

During an NMI interrupt handler the H8/300H CPU will accept another NMI interrupt request and execute the interrupt handler. During NMI interrupt handling NMI interrupt requests will not be masked
Suitable Products
H8/300H