Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Does key input detected when it occurs on falling edge of input signal?

Latest Updated:02/27/2012

Question:

Key input interrupt occurs on the falling edge of the input signal. When key input which continues "L" level input after the falling edge is generated, is key input in the meantime detected?

Answer:

If input signal falls once and then "L" level input continues, the key input after the second is not detected.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/24 (M30245)
M16C/29
M16C/28
M16C/26A
M16C/1N