Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Does V flag in CCR's changes with the data size?

Latest Updated:03/26/2009

Question:

Does V flag in CCR's changes with the data size?

Answer:

The CCR's V flag changes when an overflow is detected in the result of a signed arithmetic operation. This operation is the same for all data sizes.

However, the timing of the changes in the flag varies as follows:

- Byte: When the value is smaller than H'80 or larger than H'7F.

- Word: When the value is smaller than H'8000 or larger than H'7FFF.

- Longword: When the value is smaller than H'80000000 or larger than H'7FFFFFFF

Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902
  • Was this article helpful?