Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Definition for number of times flash memory rewriting is performed?

Latest Updated:02/27/2012

Question:

What is the definition for the number of times flash memory rewriting can be performed?

Answer:

The definition for the number of rewriting times is the number of erases for every block.
For example, if 4,096 1-word writes are performed to block 4, an 8 Kbytes block, and then the block is erased, the erasure endurance will be counted as one. With regard to products in which the programming and erasure endurance is 100 times, 1-word can be written 4,096x100 times.
However, please be aware that overwrite rewriting cannnot be performed without first erasing the area that is written to.
Suitable Products
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N