Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can you provide a simple comparison chart for 8-bit microcontrollers?

Latest Updated:02/01/2008

Question:

I am considering using 8-bit microcontrollers, but there are so many different types (product names) that I do not know which one to choose. Could you provide a simple comparison chart?

Answer:

A selection guide is available, so first refer to that. The selection guide can be viewed by inputting "78K Microcontrollers Selection Guide" in the search field on the top page of the Renesas Electronics website, then clicking  to go to the search results page, and selecting the Selection Guide from the list of PDFs displayed in the document search results field.

Suitable Products

78K Family