Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can the H8/3834 run at voltages less than 2.7V ?

Latest Updated:03/18/2009

Question:

Can the H8/3834 run at voltages less than 2.7V ?

Answer:

The H8/3834S mask version can run at voltages down to 2.5v with a 5 Mhz crystal. However the Z-TAT version will only operate down to 2.7v.The H8/38xx Super Low Power series ( eg the H8/3847 and others ) provides a functional super set of the H8/3834 and ofers 1.8 - 5.5v operation.
Suitable Products
H8/300L