Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can standby be released at the falling edge of the INT/P61 port?

Latest Updated:12/01/2011

Question:

In the uPD78932x, a 40-key key matrix is configured.
In a configuration of five input ports (KR00 to 03, INT) x 8 output ports (P80 to 85, P10, P11) = 40 keys, can standby be released at the falling edge of the INT/P61 port?

Answer:

Yes, this is possible.
Suitable Products
UPD78932x