Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can the internal pull-up function of each SCL and SDA pins be enable?

Last Updated:12/26/2017

Question:

SCL (P3_5) and SDA (P3_7) pins have an internal pull-up function. Can this function be enabled even when the I2C bus interface function is selected?

Answer:

When the I2C bus interface function is selected, the internal pull-up function of each SDA and SCL pin cannot be used.
Suitable Products
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/32C
R8C/33C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/38A