Skip to main content
Renesas Electronics Europe - Knowledgebase

Can PMW be enable for channels that had 4 TGR registers using PWM mode 1?

Latest Updated:04/07/2011


In the timer pulse unit (TPU), can two different PWM outputs be enabled for a channel that has four TGR registers using PWM mode 1?


Two different pins, TIOCA and TIOCC, are capable of PWM output. However, the output cycle will be the same because they share a counter.
To output PWM with a different cycle, please use a separate channel.


Suitable Products
H8S Family
H8SX Family