Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can I use a higher resistance Crystal Oscillator?

Latest Updated:04/07/2011

Question:

In the Clock Pulse Generator section of the manual, the table Crystal Oscillator Characteristics shows max Rs resistance. Can I use a higher resistance Crystal Oscillator?

Answer:

The resistance value and capacitance value described in the table Characteristics of Crystal Oscillator are only for reference.
Please ask your oscillator's manufacturer for matching characteristics measurements and determine resistance and capacitance values based on that data.

 

Suitable Products
H8S Family
H8SX Family