Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

'1' is written to TCSRWEbit of tTCSRWD; value '1' until '0' is written?

Latest Updated:03/26/2009

Question:

Also, when '1' is written to the timer control /status W writing enable (TCSRWE) bit of the timer control /status register (TCSRWD), is the value '1' held until the next '0' is written?

Answer:

Yes, '1' is held until the next '0' is written.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902