Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

"Any suggestions on how to get the VREF value I needed? "

Latest Updated:03/01/2005

Question:

(A/D Converter)  When I create the VREF voltage using a dividing resistor, I cannot get the VREF value I need. Any suggestions ? [2005/03/01]

Answer:

Since the VREF is connected to the internal resistor, when an external dividing resistor is used, the voltage is lowered by the internal resistor. Please adjust with a variable resistor. (#104837)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547
  • Was this article helpful?