Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What is the Product Longevity Program (PLP)?

Latest Updated:04/01/2015

Question:

What is the Product Longevity Program (PLP)?

Answer:

The Product Longevity Program (PLP) is a new initiative started in January 2014 to provide information to help customers select products with the appropriate life cycles for the duration that they plan to use them. The PLP discloses on the Renesas website the planned supply period for products that have a relatively long supply period, such as products for the industrial segment. Products participating in this program (PLP products) are managed under a special product life cycle.
Suitable Products
PLP (Product Longevity Program)