Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What does E1 or E2 mean when purchasing uPD43256BGU?

Latest Updated:04/01/2007

Question:

When I went to purchase the uPD43256BGU on a taping reel, I was asked to specify E1 or E2.
What do these terms mean?

Answer:

These terms indicate the direction in which the products are attached to the tape.
E1 means that No.1 pin display of the products faces the direction to which the tape is pulled out, and E2 means that No.1 pin display faces the direction to which the tape is winded.

Reel
side
Suitable Products