Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What's the position of products unmarked with PLP symbol on the web?

Latest Updated:04/01/2015

Question:

How are the products not marked with the PLP symbol on the website positioned?

Answer:

Products not marked with the PLP symbol are under normal life cycle management. Currently, most products for consumer applications and automotive applications are not participating in the PLP. (FAQ: 1010888)
Suitable Products
PLP (Product Longevity Program)<</td>
/div>