Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Marking part name on products

Latest Updated:08/01/2005

Question:

Marking part name on products

Answer:

The whole part name cannot be marked on small-size products, so the part name is indicated using a portion of the number or a symbol, etc.
An inspection symbol or manufacture code may also be marked in addition to the part name.
Suitable Products