Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is the PLP period counted from the start of mass production of a product?

Latest Updated:04/01/2015

Question:

Is the PLP period counted from the start of mass production of a product?

Answer:

No, the PLP period is counted from the date that the product joins the program. Note that new products can only be added to the PLP after they have entered mass production.
Suitable Products
PLP (Product Longevity Program)