Skip to main content
Renesas Electronics Europe - Knowledgebase

Do the products of Renesas Electronics regulated by RoHS Directive?

Latest Updated:11/01/2008


Do the products of Renesas Electronics contain substances regulated by the RoHS Directive?


The only substance in Renesas Electronics products that exceeds the reference levels prescribed by the RoHS Directive is lead (Pb) in old solder plated products. Therefore, lead-free products comply with the RoHS Directive.
Renesas Electronics performs in-process control for six substances restricted by the RoHS Directive, and our lead-free products are also verified to have lower lead levels than the RoHS reference value.
Renesas Electronics promotes the transition to lead-free products according to the green procurement aims.
Suitable Products