Skip to main content
Renesas Electronics Europe - Knowledgebase

Are there standards for the size, content, font size product labels?

Latest Updated:09/01/2007


Are there any standards for the size, content, font size, and so on of product labels?


There are no special regulations for label size or font size on an individual packing box or packing container.
However, there are several Japanese and international standards for the content, barcode type, and general format.

  • Japan: JEITA barcode label system (C-3 labels, etc.)
  • United States: EIA-624: Product Package Bar Code Label Standard for Non-Retail Applications
  • Europe: EDIFICE standard for unit packaging and container labels
Suitable Products
  • Was this article helpful?